This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: bq76940 alert signal to interrupt MCU input line

Part Number: BQ76940

Hi,

The design of my  firmware to handle reading of battery data is highly relied on the alert signal which could be triggered by CC_READY, or fault of bqOV, bqUV, bqSCD, bqOCD etc..

Detection of triggering of the signal is handled in an input interrupt routine like below,

//port1 interrupt service routine
#pragma vector=PORT1_VECTOR
__interrupt void isr_port_1(void)
{
  if (P1IFG & BIT5)
  {
    P1IFG &= ~BIT5; // clear interrupt flag
    bqAlert=TRUE;    <== !!!!!!!!!!!!!!!!!!!!!!!!
  }
}

In a task the reading of data is carrying out if the  "bqAlert"   flag is set, like below code,

void taskA(void)
{
  uint8_t i;
  static uint16_t time_out_counter=0;

  time_out_counter++;
  if (bqAlert==TRUE)               <==!!!!!!!!!!!!!!!!!!!!!!!!
  {
    bqAlert=FALSE;                    <==!!!!!!!!!!!!!!!!!!!!!!!!!
    bqI2CError = NO_SIGNIFICANCE;
    bqStatus.StatusByte = BqGetRegisterByte(SYS_STAT);  <==!!!!!!!!!!!
    bqI2CStatusReadError = bqI2CError;
    BqSetRegisterByte(SYS_STAT, STAT_CC_READY);    <==!!!!!!!!!!!!!!!!!!!!!!!!!

    if(bqI2CStatusReadError == FALSE || time_out_counter > 500)
    {
      if (bqStatus.StatusBit.DEVICE_XREADY == TRUE)
      {
        //for this fault data can not be trusted
        fault.BQ.bit.XREADY = TRUE;
      }
      else
      {
        fault.BQ.bit.XREADY = FALSE;
        // 250ms cycle completed
        if(bqStatus.StatusBit.CC_READY == TRUE)  <==!!!!!!!!!!!!!!!!!!!!!
        {
          // read Coulomb counter
          //int32_t cur;
          float_t cur;
          int16_t tmp;
          tmp = BqGetCoulombCounter();
          if(bqI2CError == FALSE)
          {
            if (tmp>=0)
              bqCoulomb = tmp+1;
            else
              bqCoulomb = tmp;//-1;
  .. etc.


          }
          else
          {
           //i2C error
           fault.BQ.bit.i2c = TRUE;
         }

         // read cell voltage
         uint16_t min=65535, max=0;
         for(i=0; i<NUMBER_OF_CELLS;i++)
         {
            tmp = BqGetCellVoltage(i+1);
            if (bqI2CError == FALSE)
            {
              RAM_Volt_Cell[i] =(uint16_t) gain2*tmp;
              //RAM_Volt_Cell[i] = tmp;
             if (RAM_Volt_Cell[i]<min)
             {
               min=RAM_Volt_Cell[i];
               LowestCellIndex = i;
             }
             if (RAM_Volt_Cell[i]>max)
               max=RAM_Volt_Cell[i];
         }
        else...

 The interesting thing is happening if there is bqOV/bqUV event on, the alert signal  will not generate any more, thus the battery data can not be read out,

Since recovery of such events rely on the continuous reading of battery data, like below

static void fault_bq_uv_recovery_routine(void)
{
  fault.delayCounter_1++;
  if(fault.delayCounter_1 > (5*ONE_SECOND)) //20s
  {
    fault.delayCounter_1 = (5*ONE_SECOND) + 1; //keep in
    fault.delayCounter_2++;
    if(fault.delayCounter_2 > (5*ONE_SECOND))
    {
      if(RAM_LowestVolt>=thresholds[CUV_RECOVERY_THRESHOLD])   <========!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
      {
        //criteria matched,clear faults
        fault.BQ.byte = 0x00;
        fault.SYS.byte = 0x00;
        BqSetRegisterByte(SYS_STAT, STAT_FLAGS); //clear faults and alert
        logic.regbyte_sys_ctrl2.SysCtrl2Byte = BqGetRegisterByte(SYS_CTRL2);
        //close FETs
        logic.regbyte_sys_ctrl2.SysCtrl2Bit.DSG_ON = TRUE;
        logic.regbyte_sys_ctrl2.SysCtrl2Bit.CHG_ON = TRUE;
        BqSetRegisterByte(SYS_CTRL2, logic.regbyte_sys_ctrl2.SysCtrl2Byte); //turn on FETs on bq uv recovery
        fault.delayCounter_1 = 0;
        fault.delayCounter_2 = 5*ONE_SECOND;
      }
      else
      {
        fault.delayCounter_2 = 0;
      }
    }
  }
}

I would like to know how the ALERT signal is processed in the bq76940 when a fault enent like bqUV is on, and mixed with CC_READY event?

Best regard.

  • Hi Kevin,

    Once the ALERT pin is HIGH, another fault will not cause it to toggle again.  It will remain HIGH.  To determine if another fault has triggered, check the status registers.  This will show what events and faults have occurred.

    Best,

    Andria