Hi
Could you please help to clear the application constraint as an ACOC event?
Operation: The adapter connected only
0x3C [14:11] = 150% ILIM1 = ILIM2
ICRIT = 110% ILIM2
0x37 [9] = 125% ICRIT
1. IDPM set to 1536mA,
2. IDPM set to 4096mA
Calculation:
1.150% x 1536 x 110% x 125% = 3168mA
2.150% x 4096 x 110% x 125% = 8448mA
Measurement:
1. ACOC triggered @ 5500mA (Expectation = 3168mA)
2. ACOC triggered as expectation @ 8200mA (Expectation = 8448mA)
CH1: VADP_IN; CH2: VSYS: CH4: ISYS
IDPM set to 1536mA is out of our expectations much
Thanks for your comment!
Regards
Ben