This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: the internal mechanism of the disable charge (reg01 bit4 set 0)

Part Number: BQ25601
Other Parts Discussed in Thread: BQ25890H,

Hi team,

My customer uses bq25890H+bq25601 as dual charger scheme, when charge done, set BQ25601 disable charge (reg01 bit4 set 0), power consumption (line current) is 30mA. if set the BQ25601 hiz mode to disable charge, power consumption (line current) is 15mA (Power consumption is normal), 15mA less than set reg01 bit4.


Please help the internal mechanism of the disable charge (reg01 bit4 set 0).Why is there an effect on current on the wire after only set the disable charge, which affects the EU energy efficiency certification.

(I will attach the whole register reading later)

Thanks

Best regards

Lillian