This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: TPS2121 or alternative to select between Solar and USB supply for charging li-ion battery using BQ24250

Part Number: TPS2121
Other Parts Discussed in Thread: BQ24250, TPS25947, TPS22933

I am designing a solar charger board with two inputs (Solar panel and USB). When USB cable is plugged in, the battery should charge from USB input otherwise from the Solar panel.

Solar panel input max voltage is around 9V (peak power point is 6.5V). USB input will be around 5V. The user should be able to plug in the USB cable any time to charge the battery

from USB irrespective of whether the solar panel is plugged in or not and if plugged in, producing power or not. Once the USB power is disconnected, the solar panel should charge the

battery whenever solar power is available.

I wanted to use the TSP2121 to switch between the two power supplies with USB at higher priority while using the TPS2121's "ST" pin  to inform a microcontroller of the selected power source so that

the micro can configure the BQ24250 accordingly. 

When charging from the panel, I want the BQ24250 to maintain the solar panel at the peak power point (6.5V).  Charging current could go up to 1.5A.  

Unfortunately, the TSP2121 is not in stock. Do you have any alternative part which can do the same thing ?