Hi Team,
My customer is considering use LM74502 to drive multiple MOSFET, below are customer calculation,
if Vcap > = 10*Ciss
1pcs PSMN1R4-40YLD Ciss(max)= 10413pF - > 10Ciss*1pcs = 100.413nF use VCAP=220nF
2pcs PSMN1R4-40YLD Ciss(max)= 10413pF -> 10*Ciss*2pcs = 200.826nF use VCAP=330nF
4pcs PSMN1R4-40YLD Ciss(max)= 10413pF -> 10*Ciss*4pcs = 401.652nF use VCAP=470nF
what are the maximum MOSFET we can drive?
Thanks & Regards
Eddie Chou