This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63036: ISW_MAX for IPEAK Calculation

Part Number: TPS63036

Hello,

In section 8.2.21, the equation for IPEAK includes an ISW_MAX factor. Below that, it says "ISW_MAX = Maximum average input current (Figure 6)". Figure 6 is an efficiency plot, is this supposed to refer to figure 2? Figure 2 is the max average input current limit vs input voltage.

Thanks,

Michael