This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25886: OTG pin

Part Number: BQ25886

Hi,

Please let me ask about OTG pin because I can't find its abs max and input threshold information.

  1. Is the abs max is the same with /CE?
  2. Is the input threshold and leakage current also the same with /CE?
  3. Can we control the OTG pin with 5V logic voltage directly?

Best Regards,

Satoshi