Dear Mr. TI
Hello, I have a question about UCC28180.
Q1. How to start generating PWM signal?
 Suppose there is no current flowing in Rsense at first.
 That is, Isense = 0.
 Then the -2.5x Amp output is also 0v.
 Since the gmi amp has 0v input, the output current is 0A.
 Then the ICOMP voltage is 0v, so ICOMPP = 1, and by OR4, FAULT = 1.
 The bottom right SW turns on by FAULT
 When VCOMP = 0v, M1 = 0.068x and M2 = 0[v/us] for the M1M2 generator circuit.
 Since the gmi input is still at 0v, ICOMP=0.068*0v[A], and I don't think ICOMPP will be released anytime soon.
 Please let us know if there is any error.
Q2. Regarding the M1 and M2 generation circuits
 In equation 78 on page 30, the product of M1 and M2 is related to Iout, Vout, Vin, and switching frequency.
 On the other hand, in equations 81 to 84 on page 31, M1 is expressed as a function of Vcomp.
 Also, in equations 86 through 88, M2 is also expressed as a function of Vcomp.
 By the way, Vcomp is generated when the error amplifier adds or subtracts the VCOMP voltage from or subtracts from the target value using the gmv amplifier with respect to the point where the error amplifier is balanced with 5v.
Vcomp is generated by adding or subtracting the Vcomp voltage from or from the target value with the gmv amplifier.
From this flow, I feel that Vcomp voltage is not directly related to Iout, Vout, Vin and switching frequency.
Please let me know what you mean by equation 78.
Please do so.
Thank you for your support.
				
                          
.