This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952 ADSCAN

Part Number: BQ76952


Hi

I have a query need your help.

When we use BQ76952 to get  16 channel cells voltage and 5 channel temperature, we must  get these data in  100 ms. There is a question that when we get voltage and temperature according to full scan flag of alarm status, we should take 194 ms  to confirm the full scan flag become 1 from 0.    We hope  to get voltage and temperatue according to adscan flag of alarm staus , we find that there is only 65 ms  for ad scan flag to becom 1 from 0.   Pls help us  to   confirm  that we can use ad scan flag or not.

Waiting for your reply.

Thanks

Star