This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40170: Power efficiency

Part Number: TPS40170
Other Parts Discussed in Thread: LM5145, LM5141, LM5148

Dear all,

We found that the Power efficiency of TPS40170 is low. 

When there is no load, the power consumption can be 5W or higher. Are there any energy saving mode to lower the Power consumption?

Our application is 48V to 12V conversion.

Best regards,

David