This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63610: Current rating

Part Number: TPSM63610

Hi team,

Regarding the current rating, do you mean that the over current threshold is 10A but up to 8A at DC?

Can't it be used as a 10A power supply depending on the temperature and input/output conditions?

Best Regards,