Developing a new system based on the AM3703 Microprocessor
and selected the TPS65910 for power sequencing. The primary system requirements
include the following;
Power Supply Main (VBAT) = 5.0V (switched)
Boot Time Total = 500mS max (from VBAT insertion).
There are several issues, encountered, with this system that need to be resolved.
Issue #1 Auto Power-On: Can the TPS65910 be configured for auto power-on,
using PWRON & PWERHOLD or other means, when the VBAT supply is inserted?
There is no on/off switch in the design.
Issue #2 Power-Down Timing: The system main power is switch-off at the end of the
work day. Can memory corruption or damage result in this action? A backup capacitor
is not included in the design.
Issue #3 32.768 KHz Clock Stabilization Time: The crystal clock mode stabilization
time is ~2 seconds, which is too slow. An external oscillator is a consideration, with
BOM cost and board space penalties. Is there other possibilities, such as the internal
RC oscillator, that may be viable?