This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: High power DC-DC converter with PMbus.

Part Number: UCC28950
Other Parts Discussed in Thread: UCC29002, LM5046

Greetings,

Presently we have a requirement in designing DC-DC power converter for telecom applications.

Power output: 3kW

input voltage: -48V to -72 V  

Output: 12V

Our required power density is high (62 W/in3)

Communication: PMBus

So, we want to know if we could use this IC (UCC28950) for Development.

We are also open to suggestions from your side.