I understand IrespeakOCP1 is the OCP limit for the primary side, and IsecpeakOCP1 is the OCP limit for the secondary side.
From the DS (「8.2.2.16 ISNS Pin Differentiator」) I also understand the equation to calculate IrespeakOCP1;
and from this IsecpeakOCP1 is just IrespeakOCP1 times the transformer turns ratio.
In the current setup the IrespeakOCP1 = ~6[A].
The turns ratio can't be modified, and we are looking at some other way to reduce IrespeakOCP1 to around 20~30[A].
Is there any way to modify the other values in the eq. to reduce IrespeakOCP1 and thus reduce IsecpeakOCP1?
It looks like it can be done by adjusting CISNS and CR, right...?
Regards,
Darren