Other Parts Discussed in Thread: LM74720-Q1,
Hi Team,
Can you please help answer the inquiry below?
instead of powering this IC from the voltage source that we are connecting/disconnecting, can we power the IC with an isolated supply if the isolated ground is tied to the same ground as the voltage source.
I have a 50V supply I am trying to connect/disconnect from the load. I am trying to avoid using this supply to power up the IC (charge pump inside) so I was wondering if I could use a separate isolated supply that is using the same ground as this 50V supply to power up the IC. Would i have the same switching functionality?
Thank you in advance
Regards,
Marvin