This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Maximum Temperature to be sensed by an NTC (External Temperature)

Part Number: BQ34Z100-G1

Hi,

What is the maximum temperature that can be sensed by BQ34z100-G1's External Temperature pins? Is it limited by the NTC Sensor Specifications or limited by the BQ34z100-G1 itself? 

I've not seen it cross beyond 120 °C. If I use an NTC with a maximum operating temperature of up to 300 °C, will it help to increase the range of the temperature sensing?

eg: NTC Part no. NRBG104J3435B2F
https://www.eaton.com/content/dam/eaton/products/electronic-components/resources/data-sheet/eaton-nrbg-glass-sealed-radial-lead-ntc-thermistor-datasheet-elx1105-en.pdf

Regards
Anvin

  • Hello,

    The bq34z100-G1 is tested for the operating range -40°C to 85°C. 

    Using an NTC with a maximum operating temperature of up to 300 °C does not increase the range of the temperature sensing. As long as the NTC is used within the specified range by the bq34z100-G1, the gauge will respond fine.

    Please see below recommendations for the NTC



    Note: It is ideal to use a Negative Thermal Coefficient NTC, recommended by TI for the design, and to use the recommended coefficients to make sure that the temperature measurements are accurate.

    Regards,
    Jose Couso

  • Hello Jose,

    Thanks for the information. Is there any way to modify these coefficients or any other internal parameters to measure the temperature up to  300 °C? Is -40°C to 85°C a fixed limit? 

    Regards
    Anvin

  • Hello Anvin,

    The maximum operating range is -40°C to 85°C. Anything that falls outside causes gauging problems and inaccuracy. 

    Regards,
    Jose Couso