This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: TPS55340 Design reference

Part Number: TPS55340

Hello,

Customer's actual design requirements:

Input voltage: 11.5-12.5V Output: 15V, 4A or

Input voltage: 5-13V Output: 15V, 1A

What is the recommended inductance value and input/output capacitance value? Is there any recommended circuit for reference?

Thanks!