This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27517: Schematic Review

Part Number: UCC27517


Hi Team

There is a good new that we DIN UCC27517 !

Please help confirm the SCH is ok? THX

Spec : Vin=90~264Vac / Vo=54V / Io=15A


6864.CHARGERD3.pdf

  • Hi Kygo,

    The bypass capacitors and filter on IN+ look good. As for the output stage, it is a bit unusual. The turn-off PNP circuit usually uses a diode like shown here:

    A resistor can also work though. To double-check, I simulated the circuit, and it worked well. When paralleling channels, it is better to give each FET its own gate resistor, and that is what has been done here. 

    So while I have never seen a schematic quite like this, it looks like it should work well.

    Thanks,

    Alex M.