Hello.
I working with TPS62933DRLR for one power supply. My load have the characteristic operating with 100mA constant and 1A pulsed. Similar to radio.
In webench, my simulation recommend use one inductor 3.3uH with 9A pico. Buth when I calcuculate follow the datasheet, my inductor result 3.3uH with 2A pico.
What is the difference ? Does the simulator have any safety margins or any specific details? I´m operating with 2.2MHz, my input range is 5V to 30V and output voltage is 4V.