Other Parts Discussed in Thread: UCC2897A, , PMP23253
Hello Expert,
Our customer is designing POE PD BT circuit which is configured with TPS2373-4 and UCC2897A.
In the case of FORWARD CONVERTER, I know that MAX DUTY should not exceed 50%.
They have made the board by referring to the transformer of TPS23730EVM-093.
But, we observed that the duty was occurred up to about 63% as shown below.
Is there able to occur some issue? or Is it OK?
Could you please review and give me feedback?
Also, we need to review their schematic and don't share on this thread.
Could you reply to me by e-mail and then I will send it.
My e-mail : michael.jeong@arrow.com
=============================================
PWM frequency : 205KHz
Input : 41VDC
Output : 12V/6A (72W)
Transformer : EFD25, turn ratio 2:1 (L value about 100uH)
=============================================
Best regards,
Michael