hi,
We found some problems when turing DSG MOS ON through commands in normal mode.
The steps we take as the following:
Step1: send the commands to BQ76952 and then query the DSG MOS state which is OFF.
Step2: send the commands again and then query DSG MOS State which is OFF. Here come the Problems:
Problem1: DSG MOS FET driver voltage rises to high, holdup to 1.5ms and then drop to low.
Problem2: After that, when querying the DSG MOS state from BQ76952 it shows ON, actually the MOS driver voltage is low. And the low voltage lasts for almost 246ms.
We think it should be avoid to have a pulse high voltage, and the DSG MOS state should be OFF until the driver voltage keeps high.