Other Parts Discussed in Thread: BQ40Z50
Hi team,
Here's an issue from the customer may need your help:
While charging, when SOC reaches 100%, 5th light remains flashing and does not turn solid. After charging has been switched off, the five lights are off.
Requirements:
SOC 0~20% :LED1 is flash;
SOC 20~40% :LED1 is on,LED2 is flash;
SOC 40~60% :LED1 is on,LED2 is on,LED3 is flash;
SOC 60~80% :LED1 is on,LED2 is on,LED3 is on,LED4 is flash;
SOC 80~100% :LED1 is on,LED2 is on,LED3 is on, LED4 is on,LED5 is flash;
SOC =100% :LED1 is on,LED2 is on,LED3 is on,LED4 is on,LED5 is on;
Could you help check this case? Thanks.
Best Regards,
Cherry