This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB542: SEL controller

Part Number: TUSB542
Other Parts Discussed in Thread: TUSB322I, HD3SS6126, TUSB321AI, HD3SS3220

Hello,

We plan to develop 5Gbps USB type-C UFP Device only "Memory bord" which is not integrated CPU, standalone control system.

Initially we plan to utilize TUSB320I and TUSB542, but it require I2C for TUSB542 SEL control.

 

  1. In this case, Is TUSB322I only the one candidate for CPU less Hardwired SEL control system?
  2. Is there USB controller and 2:1 MUX integrated "2 in 1" device in TI portfolio?
  3. HD3SS6126 can be alternative device for TUSB542 MUX function?

 

Regards,

Mochizuki