Please check the peripheral circuit of HD3SS3220IRNHT. I would like you to point out all the mistakes.
◆ Question
(1) Is it necessary to implement AC coupling in RX? It's not listed as a datasheet. Also, the USB3.x standard implements AC coupling only on the transmitter side.
(2) Is there any problem with the capacitance value of the AC coupling?
(3) Are there any mistakes in the circuit diagram or any parts that need to be corrected?