Hello,
I need to design a full battery management configuration (charger, fuel gauge etc.) based on the bq20z95 fuel gauge. I'm using Li-Ion 4-cell batteries. I'm thinking of using the bq24745 charger and bq294xx as the 2nd level protection IC. A few questions:
1.Is that charger recommended? If not, which charger should I use?
2. Is there an application note/block diagram for that kind of configuration?
3. The fuel gauge and the charger will share the SMBus communication. Who actually controls the charger? Is it the host or can the fuel gauge control the charger independently?
Thanks in advance.