Two questions regarding the UC1846-SP:
1) The datasheet mentions a couple different peak current values for the output used to drive the gates of power MOSFETs. Page 13 mentions 1.5A peak, 0.5A average while Page 22 mentions 2A peak. Does anyone know which peak value is correct?
2) Using the equation for setting the peak current limit on Page 12 and also taking into account input bias current, I am setting R1 and R2 as 10k and 5.9k ohm respectively to set a peak current limit of 1A. However the simulation is showing a peak current of about 1.3-1.4A. Current sense resistor is 500mohm. I had to adjust R1 to 18k obtain a peak current limit of 1A. Has anyone encountered this?