This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53647: question of TPS53647 ripple

Part Number: TPS53647


Dear Team,

Our design is: tps53647+4 phase CSD95490; Input: 12V; output: 0.89V;
The current is 48A under heavy load, and the ripple is only 10 mv, which meets the requirements; the current is 35A under no load, and the noise is more than 40 mv, which does not meet the spec requirements;
The current value is read out through the TI GUI , and the ripple is measured at the end with an oscilloscope
May I ask why the ripple is so large at no load?

I think light load get 35A from GUI is abnormal.

Many Thanks,

Jimmy