This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78000A: Temperature & Bake Duration // A0950-5635 (MPN# PTN78000AAZ)

Part Number: PTN78000A

Dear team,

What is the temperature & duration needed to bake for below part?

These are not mentioned in datasheet, please help to advise.

MPN: PTN78000AAZ

Kindly advise any issue if we send for high temperature bake for MPN: PTN78000AAZ.

We will bake in metal tray and bake out within 24 hours.
Our highest baking temperature is 120 degree.
Kindly advise if it is ok to proceed and will it cause the chip damage.
Besides that, do advise MPN: PTN78000AAZ is belongs to which package body.
Best Regards,
William