This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041A: Question about LM5041A

Part Number: LM5041A


Hello:

During 65 ℃ aging process of LM5041A of TI, PUSH and PULL output DC level. Normally, it should be 50% duty cycle,

The figure below shows the peripheral circuit diagram of the chip. After the abnormal chip PUSH and PULL pins are powered on by VCC, the output is DC level, and the voltage is about 11V.

Whether abnormal chips need to be sent to the original factory for analysis?Thanks!!!