Hi,
I am planning to use an LM3904HV for an upcoming LED lighting solution. I wanted to know if LM3904HV could drive two LED panels of 35W each. And what is the maximum power it can drive without it overheating? On an unrelated note, Should the panels be connected in series or in parallel for the best performance? This is a POE solution where the Input voltage will be between 48-54V.