Hi team
Our customer is testing LM5118, and we want to add an external dithering circuit to improve EMC performance, do you have recommended solution? Or we can just inject an external dithering voltage to RT pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Our customer is testing LM5118, and we want to add an external dithering circuit to improve EMC performance, do you have recommended solution? Or we can just inject an external dithering voltage to RT pin?
Hi Shaofeng,
Thank you for using the E2E forum.
Yes, should be possible with the LM5118.
In this case you should an R-C-R connection to the Rt resistor.
Please ensure you that you keep within the allowed frequency of the LM5118 (best is to be around 300kHz).
Best regards,
Stefan