This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156HEVM-FLY: Transformer device on LM5156HEVM-FLY

Part Number: LM5156HEVM-FLY
Other Parts Discussed in Thread: LM5156

Hi Sir,

My customer would like to replace a new transformer device on LM5156HEVM-FLY Evaluation Module to verify the function the configuration is designed to provide a regulate output of 12 V at 2 A from an input of 18 V to 36 V.

Could you help to review whether the below jump wires are correct or not?

new transformer device VP4-0075-R

VP4-0075-R.pdf

original transformer device: Wurth Elektronik / 750317933

Wurth Elektronik_750317933.pdf