Hello Team ,
i just started my learning cycle connecting the battery setup to the EVK , my battery cell are Lion cells (3 cells) part number US18650VTC5A so the chemid is 0x2161
.programmed the chemid started the learning cycle.
1. Discharge battery to empty. -> Actually i have took C/10 Rate -2600MAh /10 = 260 MA = 0.260A , i have attched my test setup screen shot also. for your reference.
Term voltage set as 8995 mv , but before reaching the voltage range the gauge report 0 % , before reaching the point VOK and RDIS bit is cleared and RESET flag is set , as per my understanding RESET flag will set after the relax mode.?
what was the reason for the failure of my learning cycle ? Can i able to proceed with this setup for charging ? or i need to start again. i attached log files for your reference
Whether balancing circuit is available in EVK setup ???