This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: the function relationship between FCC and temperature

Part Number: BQ28Z610-R1


Hello,

What's the function relationship between FCC and temperature? Why we find sometimes termperature rise and FCC rise,but other times the same temperature rise and FCC decrease.

  • Hello Ran,

    FCC is highly depended on temperature and load. Full Charge Capacity is the total amount of charge that the battery can deliver to a system for a specific set of conditions (average load, temperature).

    If a change in temperature is greater than 5C, then FCC is likely to change. 

    but other times the same temperature rise and FCC decrease.

    Please send a log file to provide specific feedback.

    Regards,
    Jose Couso