Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO
Hello Team ,
i am using sony Lion cell battery for my learning cycle, US18650VTC5A .
Flashed the chemid and configure the paramters.
Could you please confirm whether these parameters are enough for my learning cycel any updation is required or not ?
Charge term taper current : 140 MA
Dicharge current Threshold : This is the current threshold above which the gauge detects that it is in discharge mode : 30MA
Chg Current Threshold : This is the current above which the gauge detects that it is in charge mode : 40 MA
Quit Current : This is the threshold that determines that the gauge enters relax mode : 15MA
Term voltage : 3x3v = 9v
Design Voltage : 3 * 3.6 v = 10.8 V
Design capacity : 2600 MAh *3 = 7800 MAh