Other Parts Discussed in Thread: LM5145-Q1, LM25148-Q1, LM25141-Q1, LM5146
Hi Team,
Could you please review the below LM5146-Q1 schematics of our application board. here are the design requirements for our design
Vin minimum = 9V
V typical = 12V
V maximum = 16V
Output current = 10A
Output Voltage = 3.7V
Switching Frequency = 255khz

In addition to above could you also suggest to have EMI Filter circuit for CISPR25 class 5.
Regards,
Chaitanya