This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR64010: Looking for a DC-DC converter that can output 40V say 1.5A

Part Number: LMR64010
Other Parts Discussed in Thread: LM5176, LM5157, LM51581

Hi Experts,

Our customer is looking for a DC-DC converter that can output 40V say 1.5A. This is for a pulse-loading application.
He has located LMR64010XMFX/NOPB. This seems to be a good part, but is there a version that gives slighter higher current at 40V. This looks like can give 200 mA at 40V.
And also the input Max. is 14V. Do you think there is a solution for a slightly higher Vin max.? He also mentioned that high switching freq. is desirable for smaller comp. As this is for a high-volume production the cost needs to be small.

We also see LM5176 but very costly for the customer. He said that the design is for high-volume production and the cost target for the entire design (Trackpad) is $10. Hence, he needs a cheap and simple solution.

We also came across LM5157 as well. Do you think it is a good part? Please advise. Thank you

Best regards,

Gerald