This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24210EVM-678: VBAT never goes above 4.0V

Part Number: BQ24210EVM-678


I am following the below from the evm user guide

2.4.2 Charger Enable and Battery Detection

Connect JP1; Connect 2-3 of JP7 (Charger ON/MODE High)

Measure → V(J4(VTSB)) = 2.2 V ± 300 mV

Connect 2-3 of JP5 (Internal TS);

Adjust R6 until V(JP4-1) = 0.7 V ± 200 mV

Measure → V(J2(VBAT))=4.2 V ± 200 mV

Observe → D1 (PG) ON, D2 (CHG) OFF

On my evm i measure the .7V and the 2.2V, but every time I check VBAT I only see 4.00V. I understand that it is +/- 200mV, But I am 

curious if vbat can be trimmed up? if so how?

Thanks,

John