Hi,
The terminals OUT1 to OUT8 are used to operate the LCD panel with an amplitude of 15 V and 60 Hz.
Therefore, I will attach the output voltage and current waveform of the OUT terminal in the worst case.
Could you tell me if there is a problem with the current capacity of the OUT terminal?
According to the D/S, the continuous output current is 30mA typ, but the LCD panel is instantaneously
charged and discharged with a current of 60mA.
Best regards,
Hiroshi