Other Parts Discussed in Thread: LM3409, TPS92641
We are looking for a suggestion for suitable parts for a new design.
Design requirements for the new LED driver:
Buck
V(in-nom) 48V
Vf(led) 30-40V
I(led) 6A
f(PWM) 20kHz
The configuration is 6 separate LED channels (LED colors). All channels are PWM controlled in real-time to produce the desired spectrum and most of the channels are active at any given time.
The Vf of the strings are 30-40V as mentioned above and there may be parallel strings.
We need to dim to a low brightness (0.1%) without noticeable change to the spectrum (we have techniques to increase linearity at low brightness). Hardware linearity to 0.1% of a 20kHz PWM duty cycle is probably out of the question. What is the shortest current pulses achievable?
We are not new to LED drivers. Our existing designs are mostly based on the LM3409 from TI. We now need more current than we can get from the LM3409.
The advantage of the LM3409 is that it is fast and can be made more precise with a shunt FET.
We are looking for a suggestion for suitable parts for this new design.
We will require higher power in upcoming products and it would be great if the same part could be used.