Other Parts Discussed in Thread: UCC2806
Hi Everyone,
I'm using the UCC28C42 Peak Current Mode Controller and I tie the RT/CT pin directly to the output of the external clock (it can handle the sink current of the controller).

Can I drive the RT/CT with a 50% duty cycle?
Will the internal oscillator clip the time duration of the external oscillator?
If we take for example the UCC2806 the duration of the sync controls the time both output are off. does the same happen here wit the UCC28C42?
Thank you.