Other Parts Discussed in Thread: TPS62933, TPS54202
I have designed a buck converter circuit using TPS5402. The schematic of the circuit is shown below:
The input voltage is 15V and we need 5V regulated output. The output current requirement is 1.5A. The designed circuit works fine till 0.7A loading condition (provided using electronic load at constant current mode). But beyond 0.7A loading condition, the output voltage starts dropping below 5V. Please suggest me some suitable solution for this problem.