Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Hello,
I am just testing with the TPS65987EVM and the Application Customization Tool for my new project.
The target design should be a USB-C design with a DFP USB3.1 (Host) for e.g. a powered USB Hub or a USB-C docking station and a 20V 3.5A sink function for charging the host.
For this design I think I have to work with a DRP Port Configuration – right.
My question is, where can I define, that this USB-C port in Dual Role Port mode is only a DFP for USB (Host - USB20 and USB3.1) and cannot switch over to a UFP (Device)?
I doesn’t find any right option in the configuration tool.
Regards Markus