This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1:40z50-R1 4.35V charging 4.2V batteries.

Other Parts Discussed in Thread: BQ40Z50-R1, BQSTUDIO

部件号:BQ40Z50-R1

您好,专家: 背景:
1.由于4.35V圆柱形电池停产,必须使用4.2V电池;
2.请勿修改主机中的4.35V/节充电时调试电量计;
3.应用程序为4S2P组合结构。
4.4.2V电池的正常规格是3400mAh最小容量。
问:如何学习在4.35V/节的基础上为4.2V/节电池充电?
尝试解决方案:
1.过充保护电压设计为4.2V,充电为4.35V,这意味着在充电过程中不会有恒压级,并且会出现容量损失。
2.由于充电条件的变化,化学ID从之前的2708-->2250重新制作。
3. 分析更新状态未跳转到 05,表示 Qmax 未更新。
4.使用老化柜记录电池容量约4600mAh,并将设计容量修改为4400mAh。
5. 参考《TI 电量计应用指南》中的 SOH 段落,修改 Qmax 上限值可以解决类似的问题。
原文如下:“还应注意的是,降压后可用容量变小。为了使SOH显示器达到合理的水平(例如,工厂显示器为100%),应根据实际可用容量填写设计容量。例如,有一个服务器BBU电池根据电池规格,充电到3000V时的标称容量为4.2mAh,但充电到4.0V时只有2150mAh,因此电量计的参数设计容量应填充2150mAh。如果装满3000mAh,SOH出厂时不会到达它。100%.并且需要注意的是,如果新的DesignCapacity远低于原来的设计容量,请联系TI技术支持或E2E技术论坛修改Qmax上限(默认值为130%,表示Qmax更新限制为DesignCapacity的130%),以免影响Qmax的更新。这个设计容量没有明确的指标“大量降额”。一般的经验标准是将降额差除以新的设计容量。如果比率超过 30%,则应增加 Qmax 上限。例如,(3000-2150) / 2150 = 40% >30%,您需要将 Qmax 上限调整为 230%。6. 基于上述,(3400*2-4400)/4400≈54.5%>默认值30%,估计A值为235%。
附加 gg 文件