Hello,
Is it okay to select a high impedance (1Mohm and 39kOhm) as R1 and R2 in the datasheets typical application figure in order to minimize leakage current? The recommendation of "Select (R1 + R2) such that current through resistors is around 100 times higher than the leakage through OV pin" would be true in this case.
Would this high impedance have any affect on the OV response time?
Regards,
Viktor