Hi All,
In LM74700' datasheet page 18 (Selection of TVS Diodes for 12-V Battery Protection Applications), it mentions that pulse 1 is -150V with 10 ohm impedance, while when I check ISO7637 pulse 1 is -100V with 10 ohm impedance.
and it says we need a TVS with clamping voltage of less than 44V, while SMBJ33CA’s clamping voltage is 53,3V(breaking voltage is 42,2V).
So the question is that are these information correct or did I miss some points?