Dear Sir.,
I have a battery charger developed with the LM5175, the loop bandwidth is lower than 1kHz (about 400Hz) to achieve stability for a large input and output voltage and current range. My switching frequency is 100kHz in DCM with RMode=49.9k and Cslope of 100pF.
I tried to use a Dither capacitor of 10nF value, but when the charger works in Buck-Boost and Buck mode the output oscillate at about 5kHz (Dither frequency) and I can hear a noise from the charger, if I remove the Dither capacitor the oscillations disappears and the noise too.
In my case where the loop frequency so low, does it makes sense to use the Dither function? If yes, What should be the correct Dither frequency to use in my case?
What should I do? Should I try to increase the loop frequency?
Please can you help me?
Thank you in advance.
B.R.
Francesco Pierannunzi