Customer feedback LM5180 input 48V output 15v & 7.5v,
the following waveform is loaded at 15V&30mA +7.5V&100mA SW voltage waveform,
the switching frequency is not fixed at 12kHz, but mixed with about 350kHz, what is the reason?
ps: When 15v outputs 100mA current, the switching frequency can be stabilized
Transformer parameters: primary side inductance 21uH, leakage inductance 0.5uH, turns ratio 13:4:4.
Below is the actual schematic from the customer: