Other Parts Discussed in Thread: TUSB320LI,
Can TPS25750 be combined with TUSB320LI in the same USB port circuit to support USB-OTG function with power delivery (sink and source) through Type-C connector? Can both of these be connected to the same CC1/CC2 lines without interfering with each other? We used TUSB320LI for detection of DRP function (host/slave) and we would like to add TPS25750 to add support for power delivery (both source and sink). Is this possible?
Thanks
Branislav