This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: VOUT Spec inquiry

Part Number: TPS1H100-Q1

Hi team,

 

In TPS1H100-Q1, the max. spec of Vout is same as the input (48V), but a customer asks about the min. spec of Vout.

Is the min. Vout same as the reverse polarity voltage(-18V) or Vds,clamp(-70V)?

 

Thanks,

Sam Lee

  • Hi Sam,

    The output pin is rated to withstand the reverse polarity voltage in long time scale events and is rated to handle up to the maximum negative voltage experienced during a inductive clamp event(clamped by Vds). The customer is not meant to drive the device in any other condition that can cause a negative voltage on the output pin.

    Thanks,

    Shreyas